Technical FAQs

Ask a Question

What is the operating temperature for a M251 / LMC058 controller?

The ambient operating temperature for a M251 or LMC058 controller is: -10 to 60 degrees C (14 to 140 degrees F) for horizontal installation or -10 to 50 degrees C (14 to 122 degrees F) for vertical installation.
Was this helpful?
What can we do to improve the information ?