Technical FAQs

Ask a Question

What causes Concept error "-4017 Link failed"?

  The link cannot be created during text import & build of an FBD section.

    There is an unknown data type because there is a missing .DTY file.
    Verify that Concept has access to any needed .DTY files.  They should reside in either the C:\Concept\LIB folder or the local \GLB folder.

Was this helpful?
What can we do to improve the information ?