Technical FAQs

Ask a Question

What causes Concept error message "-1448 Parameter ‘Continue after’ wrong by GetValueService"?

  Problem animating online in Concept.

Product Line:
   Concept Programming Software

  The IEC service, which is used to update values for animation, failed due to a fault in the communication between the PLC & PC

   Check communications between the PLC and the PC.
   Minimize animation.  Animate only one to three sections in parallel, including the RDE, LL984 and IEC sections.
Was this helpful?
What can we do to improve the information ?