Technical FAQs

Ask a Question

What Telefast base is used with the BMEAHO0412 HART module?

The ABE7CPA21 is used with the BMEAHO0412  HART module using the BMXFCA150/300/500 cable.
Was this helpful?
What can we do to improve the information ?