Technical FAQs

Ask a Question

What does Unity Pro 8.0 provide for network security?

Unity Pro 8.0 provides the capability of disabling FTP/TFTP and HTTP access to an Ethernet network. When configuring the Ethernet network there are two options to disable or enable the FTP/TFTP and HTTP access.
Was this helpful?
What can we do to improve the information ?