Technical FAQs

Ask a Question

What's the refresh time of Position output in M218 PTOsimple FB?

The refresh time of Position output in PTOsimple FB depends on the numbers of PTOSimple and system scan time. If only one PTOsimple FB is used in applicatoin ,the refresh time is one cycle time of PLC.
Was this helpful?
What can we do to improve the information ?