Technical FAQs

Ask a Question

What CM2000 Datalogs are supported in ION Enterprise?

Issue
Data logs greater than 5 on the CM2000 series are not showing up in ION/SPM/PME.

Product Line
ION Enterprise, Struxureware Power Monitoring Expert

Environment
Log Setup on CM2000 series meters. 

Cause
Data Log 14
Onboard data log 14 is reserved for MV90 logging. This will allow an MV90 specific application to use this log without any possibility of conflict with ION/SPM/PME.

Data Logs 5-13
Onboard data logs 5 through 13 are not to be supported by ION/SPM/PME.  Generally, there is only enough RAM available on the device for 2-3 logs.  By not supporting logs 5-13, the need to check to see if these logs are active and allow the user to configure logging that will not be picked up by ION/SPM/PME.

Resolution
There is no workaround for this. Will have to use logs 1-4 on the CM2000 series meters for data logging. 
Was this helpful?
What can we do to improve the information ?