Technical FAQs

Ask a Question

I have SoMachine installed on my PC and when I install SoMove both programs have issues with the DTM libraries, why?

Users of SoMachine that wish to install SoMove need to follow these steps to avoid DTM library issues.

If you already have SoMachine installed and it is working correctly do the following
1. Install SoMove but DO NOT INSTALL the DTM libraries. Installing the libraries will cause broken links which will effect SoMachine and SoMove
2. After installing SoMove run the Schneider Electric Software Update tool found in the programs directory.

If you have already incorrectly installed SoMove and now find that it does not work and SoMachine is also not working you must do the following.
1. Completely remove SoMove using the Unistall feature in Add/Remove programs
2. Remover the DTM libraries in Add/ remove programs.
3. Navigate to the folder C:\Program FIles\Common files\Schneider Electric shared and delete the lexiumDTMLibrary folder
4. Launch the Schneider Electric Software Update tool found in the programs directory and update.
5. Next launch SoMachine and verify it is functional.
6. Close SoMachine 
7. Install SoMove but DO NOT INSTALL the DTM libraries.
8. Launch the Schneider Electric Software Update tool found in the programs directory and update.

Both programs, SoMachine and SoMove, should now be working properly.
 
Was this helpful?
What can we do to improve the information ?