Technical FAQs

Ask a Question

What type of signal is provided from the PTO output of Lexium 32 drives?

The PTO signal from LXM32 is RS422 compliant.  It provides an A B type signal plus an index pulse.
The signal level is 5 volt.
The resolution of the PTO output can be configured via the ESIM_scale parameter within Lexium 32 

Attached you will find the technical data information for the PTO signal as seen in the manual for LXM32C.  Note that the specifications are the same for LXM32M
Was this helpful?
What can we do to improve the information ?