Technical FAQs

Ask a Question

How to get the Backup Battery for Flex PC Box (ref: MPCYN00BBU00N)?

The Backup Battery for Flex PC BOX (ref: MPCYN00BBU00N) was never commercialized as spare part.
In order to get this product, it is necessary to contact country services who will order by email to EU-MRO-SERVICES including the Part Number AAV90017 like below:
Our Material No. Material Description
MPCYN00BBU00N AAV90017 Backup Battery for Flex PC BOX

The reference AAV90017 is very important because it is the only one known in our process.
The lead time is about 2 months.
Was this helpful?
What can we do to improve the information ?