Technical FAQs

Ask a Question

How to change the device address on a MiCOM using Easergy Studio?

Issue  
Need to change the device address on a MiCOM using Easergy Studio

Product Line  
Easergy Studio (MiCOM S1 Studio)

Environment  
Easergy Studio

Cause   
Device address needs to be changed.

Resolution 
In S1 Studio right click on the device and select "Supervise Device".



Once the "Supervise Device" box popup select "Device address"



The "Device address" box will popup.  Select or type in the address for the MiCOM and click "Change".

 
 
Was this helpful?
What can we do to improve the information ?