Technical FAQs

Ask a Question

How to change the time and date on a MiCOM using MiCOM S1 Studio?

In S1 Studio right click on the device and select "Supervise Device".



Once the "Supervise Device" box popup select "Date and time"



The "Date and time" box will popup with two ways to change the time.  One is to select the time and date, then click change.  The second option is to send the pc time and date to the device.  
This done by just clicking "Send current date and time"


 
Was this helpful?
What can we do to improve the information ?