Technical FAQs

Ask a Question

How to open or close a breaker on a MiCOM using MiCOM S1 Studio (Easergy Studio)?

Issue     
Need to close the breaker remotely.

Product Line  
MiCOM P12x
MiCOM P14x

Environment  
Software

Resolution

NOTE : Please follow extreme caution while opening and closing a Circuit breaker as this may cause irreparable damage to property and may also harm people working on the gear. 

In S1 Studio right click on the device and select "Supervise Device".



Once the "Supervise Device" box popup select "Breakers"



The "Breakers" box will popup. Choose the breaker and click "Open breaker" or "Close breaker".

Was this helpful?
What can we do to improve the information ?