Technical FAQs

Ask a Question

Does Lexium SD328 provide a pulse output signal?

No, SD328 does not have a pulse output.

Customers may have an application using SD328 in which the need a pulse signal from the SD328 to provide feedback to the PLC.
There is no pulse output available from SD328.
If you must have a pulse output you must use an external encoder or use a BRS stepping motor with encoder to provide the pulse signal.
Was this helpful?
What can we do to improve the information ?