Technical FAQs

Ask a Question

What is the number of BMXNOM0200 modules supported with M580 CPU's in general

A BMXNOM0200 consumes 1 application specific channel per configured port (ie max 2).
A max of 16 NOMs can be used in the local rack as long as the max number of application specific channels (depends on CPU type) available for the local rack is not exceeded.
A max of 2 NOMs can be used in the drops supporting a BMXCRA31210 or BMECRA31210, as long as the max number of application specific channels (36) available for the drop is not exceeded.
Globally, a maximum of 16 BMXNOM0200 modules has been tested in a M580 system. It is highly recommended to not overpass this limit.

 
Was this helpful?
What can we do to improve the information ?