Technical FAQs

Ask a Question

Does Lexium 23 Plus pulse input accept 24 volt and 5 volt logic?

No, Lexium 23 plus pulse and direction inputs are designed for 5 volt logical signals only.
If you want to use 24 volt logical outputs from the PLC then you must add a 1k ohm series resistor in line with the signal to drop the voltage to an acceptable level. (see attached example diagram)

Was this helpful?
What can we do to improve the information ?