Technical FAQs

Ask a Question

How can I correct Concept error message "-905 Invalid sysinfo component"?

  Error is displayed when trying to open a project in Concept.

Product Line:
   Concept programming software

   There may be a missing project file.

   Verify that the project.prj file is present.
   Check for a valid project path.  Should be 29 characters or less.
   Make sure none of the project files are read only.

Was this helpful?
What can we do to improve the information ?