Technical FAQs

Ask a Question

Purchasing and support of the Quantum PLC DeviceNet Scanner SAC-QDNET-010 -

The Quantum module part number 140-SAC-QDNET-010 is a DeviceNet interface module and is made by one of Schneider Electric Collabortaive Automation Partner ( CAPP) AVG Automation.
It is sold and supported directly by the partner and not through a Schneider Electric distributor
Link for product: http://www.autotechcontrols.net/devicenet/index.htm

The contact details for AVG Automations:
AVG Automation
343 St. Paul Blvd.
Carol Stream,  IL  60188
United States
Toll Free: (1) 800-TEC-ENGR (832-3647)
Fax: (1) 630 668-4676
Email: info@avg.net
Website: www.avg.net


 
Was this helpful?
What can we do to improve the information ?