Technical FAQs

Ask a Question

Is the Magelis HMIS5T Control Unit interchangeable with any Front Unit?

Issue:
Is the Magelis HMIS5T Control Unit interchangeable with any Front Unit?

Product Line:
HMIS5T, HMISTU655, HMISTU855

Environment:


Cause:


Resolution:
Yes. the new HMIS5T Control Unit is interchangeable with any Front Displays and Size.

The old HMISTU655 Control Unit is compatible with the old HMISTU655 and the new HMIS65 Front Displays.

The old HMITU855 Control Unit is compatible with the old HMISTU855 and the new HMIS85 Front Displays.
Was this helpful?
What can we do to improve the information ?