Technical FAQs

Ask a Question

Is there a whitepaper on setting up the HMISTO/STU Time Synchronization from a Unity Pro or Twido controller?

Issue:
Is there a whitepaper on setting up the HMISTO/STU Time Synchronization from a Unity Pro or Twido controller?

Product Line:
HMISTO, HMISTU, Vijeo Designer

Environment:


Cause:


Resolution:
Attached is a whitepaper on setting up the HMISTO/STU Time Synchronization with Unity Pro or Twido controller.
Was this helpful?
What can we do to improve the information ?