Technical FAQs

Ask a Question

How can one read the status of an input in Lexium 32 assigned as a freely available input?

Issue: Many times customers would like to use the inputs on a Lexium 32 as general purpose inputs.  Thus there is a need to read the status of these generic inputs for use in the process.


Product Line: Lexium 32


Environment: None


Cause: Application need


Resolution:  One can read the parameter  _IO_DI_act to know the status of all inputs even if they are assigned as freely available.
Was this helpful?
What can we do to improve the information ?