Technical FAQs

Ask a Question

Which current rating on the drives label should I use?

Issue:
Labeled current ratings.

Product Line:
All drives

Environment:
All models and serial numbers

Cause:
None

Resolution:
The Output current rating listed on the drive label is the motor current listed by the National Electrical Code standard.  This is the current rating that should be used.
Was this helpful?
What can we do to improve the information ?