Technical FAQs

Ask a Question

The catalog for 12-inch Universal Panel PC, HMIPUF6A0701, specified it as an Intel® iCoreTM 3rd generation 827E low power. What is the processor speed?

Issue:
The catalog for 12-inch Universal Panel PC, HMIPUF6A0701, specified it as an Intel® iCoreTM 3rd generation 827E low power.  What is the processor speed?

Product Line:
Universal Panel PC

Environment:


Cause:


Resolution:
The 12-inch Universal Panel PC uses the Intel® Celeron M 827E 1.4GHz processor.
Was this helpful?
What can we do to improve the information ?