Technical FAQs

Ask a Question

What are the dimensions of the M241?

The dimensions for the M241 are as follows:

Width  5.91 inches
Hight   3.72 inches
Debth  3.44 inches
Was this helpful?
What can we do to improve the information ?