Technical FAQs

Ask a Question

Do we have a driver in Vijeo Designer for the IDEC MicroSmart Pentra?

Issue:
Do we have a driver in Vijeo Designer for the IDEC MicroSmart Pentra?

Product Line:
Vijeo Designer

Environment:


Cause:


Resolution:
Vijeo Designer v6.2 does not have a driver for the IDEC MicroSmart Pentra.  But from the specifications of the MicroSmart Pentra, see link below, it does have built-in Modbus Master and Slave ports.
 
https://www.idec.com/gben/products/Catalogs/PLCs/MicroSmartPentra/overview.html
Was this helpful?
What can we do to improve the information ?