Technical FAQs

Ask a Question

What are the part numbers for the connection cables (Power and Encoder) for a BRS3ACW851FCA 3-phase stepper motor?

Title : Part numbers for the connection cable for a BRS3ACW851FCA motor

Issue : Customer interested in quoting the motor along with the cables

Product Line : SD3, BRS, Stepper motors

Environment : Not Applicable

Cause :  possible sales opportunity

Resolution: The part numbers for the Power and Encoder cable for BRS3ACW851FCA 3-phase stepper motor are as follows:
Power Cable : VW3S5101Rxx (4 x 1.5 shielded;  motor end with 6- pin circular connector, other cable end open) where xx = 30, 50, 100, 150, 200 are lengths in metres
Encoder Cable : VW3S8101Rxx (shielded; motor end with 12-pin circular connector; other end 12-pin Molex connector) where xx = 30, 50, 100, 150, 200 are lengths in metres
Was this helpful?
What can we do to improve the information ?