Technical FAQs

Ask a Question

What is the fuse requirement for the BCPM Voltage inputs?

Issue
A user is installing a BCPM and needs to know what type of fuses are needed on the voltage inputs.

Product  Line
BCPM 

Environment
BCPM Installation

Cause
The BCPM installation guide specifies that voltage lines on the meter must be equipped with fuses but fuse specifications are not listed.

Resolution
The recommended fuses for the voltage inputs on a BCPM are 1/2 amp slow blow fuses.
Part number EMFP3 is for a 3-pack of the recommended fuses.






 
Was this helpful?
What can we do to improve the information ?