Technical FAQs

Ask a Question

How do I obtain additional device licenses for Power Monitoring Expert?

A user can not enable more devices than the number of activated device licenses.
Product Line:
Power Monitoring Expert 7.2.x
PME Active Device Limitations
A user requires additional device licenses in PME.
Device licenses can be ordered by contacting sales at (615) 287-3535 or emailing them at "".

Please note that technical support does not have a tool for generating temporary device licenses for users.
Was this helpful?
What can we do to improve the information ?