Technical FAQs

Ask a Question

What is the chemical resistance for the Magelis HMIGTO/STO operator interfaces?

Issue:
What is the chemical resistance for the Magelis HMIGTO/STO operator interfaces?

Product Line:
HMISTO, HMIGTO

Environment:


Cause:


Resolution:
Attached is the chemical resistance on the HMIGTO/STO targets
Was this helpful?
What can we do to improve the information ?