Technical FAQs

Ask a Question

Does Schneider Electric offer a commissioning cable for Lexium Integrated Drives when using Lexium CT commissioning software?

Yes, Schneider Electric offers a commissioning cable designed to interface with the RS485 port of all Lexium Integrated Drives.
The part number of the commissioning cable is VW3L1T000R30

Please note that this cable (VW3L1T000R30) must be used in conjunction with the Schneider Electrics USB to RS485 adapter ( TCSMCNAM3M002P ) or a similar RS485 adapter which has the correct pin assignment to mate with the RJ45 gender changer that comes supplied with VW3L1T000R30.

See the attached PDF file for more details.
Was this helpful?
What can we do to improve the information ?