Technical FAQs

Ask a Question

What is Micom Z-Graph Software and where can it be download it from?

Issue
What is Micom Z-Graph Software and where can it be download it from?

Product Line
Micom P440

Environment 
Microsoft Windows/ Micom S1 Studio

Cause
Unable to find Micom Z-Graph software and its documentation.

Resolution
Micom Z-Graph software allows downloading distance protection settings from the relay and displaying the tripping characteristic for all 4 groups. The user can modify the distance settings and upload the new configuration into the relay. Conversion to Rio Format, and an Expert Tool for analysis is available. This software only works with Micom P442 Relay.




The software can be download from BOX at the link below:
https://schneider-electric.box.com/s/8o6oamed3c0li9eln30rh805sc2njo2p
Was this helpful?
What can we do to improve the information ?