Technical FAQs

Ask a Question

What are the dimension of the ATV312HU75M3?

What are the dimension of the ATV312HU75M3?
 
Issue:
What are the dimension of the ATV312HU75M3?
 
 
Product Line:
ATV312HU75M3, ATV312HU55M3, ATV312HU55N4, ATV312HU75N4, ATV312HU55S6, ATV312HU75S6

Environment :
ATV312 frame size 8


Cause:
Dimension

Resolution :
Width  - 7.09"   180 mm
Height - 9.13"     232 mm
Depth - 6.77"     172 mm

The jog dial add .024” (6 mm) to the depth of the VFD
Was this helpful?
What can we do to improve the information ?