Technical FAQs

Ask a Question

How to use a Launching Module in the VIP to generate a Repgen Report

In newer Operating Systems after Windows Server 2003 the VIP cannot lauch a repgen session to generate a report.

ION Enterprise 6.0.x
SPM 7.0.x
PME 7.2.x

Windows Server 2008, 2008 R2, 2012, 2012 R2
Windows Vista, Windows 7, Windows 8
Designer Application

A Microsoft security feature called session 0 isolation prevents services from interacting directly with the desktop.

Use a lauching module in the VIP to run a batch file that starts a scheduled task that runs the Repgen program.
Refer to the PDF attached to this article for details to setup the task, batch file and launching module.
Was this helpful?
What can we do to improve the information ?