Technical FAQs

Ask a Question

What is the replacement for TSXSUP1051 Power supply?

Title:
Replacement part number

Issue:
Parts become obsolete and need to have some comparable replacements for customer sto be able to use the products in the field.

Product Line:
Telemecanique TSX

Environment:
None

Cause:
Obsolescence

Resolution:
TSXSUP 1051 is a 24V, 5A power supply also used for TSX Premium amongst others.  This is now obsolete. A comparable replacement is
ABL8DCC05060.
Was this helpful?
What can we do to improve the information ?