Technical FAQs

Ask a Question

Is it possible to renew the 90 Day Trial License in PME 7.2.x?

Issue: 
A user would like to renew or extend the PME trial license.
 
Product Line: 
Power Monitoring Expert 7.2.x
 
Environment: 
Power Monitoring Expert 7.2.2 Licensing and Activation
 
Cause: 
The 90 day PME trial license is activated during the PME installation and will expire after 90 days.
 
Resolution/Workflow: 
It is not possible to extend or renew the PME trial license on a computer.

Once the trial license has expired it is not possible for the trial licence to be reactivated or renewed on the machine. 
Was this helpful?
What can we do to improve the information ?