Technical FAQs

Ask a Question

Cannot open MDI device driver after upgrading to SPM 7.0.1 from SPM 7.0

Issue:
After upgrading from SPM 7.0 to SPM 7.0.1, user cannot open the .ion file in the Modbus Device Importer (MDI)

Environment:
Upgraded from SPM 7.0 to SPM 7.0.1

Product:
SPM 7.0.1

Cause:
The MDI tool is looking for a specific string in the .ion file that was not included in SPM 7.0

Resolution:
Need to add content to the .ion file before opening with the MDI.

Change the first line of the .ion file from <?xml version="1.0" ?> to  <?xml version="1.0" encoding="UTF-8"?>
 
Was this helpful?
What can we do to improve the information ?