Technical FAQs

Ask a Question

How do I copy the parameter settings and third party motor settings from a Lexium32M drive into another Lexium32M drive?

Attached to this Knowledge article you will find a PDF file which provides step by step directions for copying the parameter and third party motor setting from a Lexium 32M drive into another Lexium 32M drive.
This process will be required if the need to replace a damaged or defective Lexium 32M drive occurs.

Please note that the replacement hardware must be the same model and power class of the drive being duplicated.
The replacement drive must also have identical optional modules installed as those found in the original drive.

See the attached PDF file for instructions.
Was this helpful?
What can we do to improve the information ?