Technical FAQs

Ask a Question

Can I use the BMXEHC0800 HSC card with the Unity Pro simulator?

No.  The BMXEHC0800 high speed counter card has it's own CPU and memory separate from the controller.  The counter value is updated independently from the controller scan. At the end of each scan, the controller reads the counter value from the HSC.  Unfortunately you cannot use the BMXEHC0800 with the simulator.
Was this helpful?
What can we do to improve the information ?