Technical FAQs

Ask a Question

For ATV61 / ATV71 sizes 14 and 15, Can eyebolts be attached to the drive?

Issue:
For ATV61 / ATV71 sizes 14 and 15, Can eyebolts be attached to the drive? Where would this eyebolt attach to the drive? Is there an instruction sheet for this lifting method?

Product Line:
ATV61, ATV71

Environment: 
Frame size 14 and 15

Cause:
Installation

Resolution:
In the drive there are 2 screws M16. These screws must be removed to insert the eyebolts.
See attachment
Was this helpful?
What can we do to improve the information ?