Technical FAQs

Ask a Question

Is there a sleep mode in either ADVC2 or PTCC controller?

Issue
Is there a sleep mode in either ADVC2 or PTCC controllers that will make it go into sleep mode if power has not been restored for a certain period of time

Product Line
ADVC2 controllers
PTCC controllers

Environment
Backup battery

Resolution
There is not sleep mode but there are "Low Power Mode" and Shutdown mode.
- When DC volt is less than 18V within 8ms (Eg Trip/close in battery condition) controller goes into Low Power Mode where Radio supply is shut down, capacitor charge is at lower rate.
- If DC voltage is less than 20V for more than 200ms, controller goes into shutdown mode

 
Was this helpful?
What can we do to improve the information ?