Technical FAQs

Ask a Question

Is there a way to determine the OS version of a Unity CPU ?

Yes. System Word %SW14 will provide the Unity user with the OS version currently running in the Unity CPU.
The value that you read is in decimal. Please convert it to hex in order to see the version number.

Using an M340 with OS version 2.50 as an example we see a decimal value of 592 in %SW14.
When converted to hex we see a value of 250, or version 2.50.


Product Line: M40, Quantum, Premium, Unity ,


Environment: n/a


Cause:n/a


Resolution:n/a

 
Was this helpful?
What can we do to improve the information ?