Technical FAQs

Ask a Question

PME 7.2 Data Center Edition - Branch Circuit reports missing

Issue:
After PME 7.2 Data Center Edition is installed there is no report under Branch Circuit Energy Reports and Branch Circuit Power Reports.



Product Line:
Power Monitoring Expert 7.2.x Data Center Edition

Environment:
Power Monitoring Expert 7.2.x Web Applications - Reports

Cause:
These reports are not included in the base version of the software.
The following reports are included in optional add on modules for PME7.2

1. Generator test
2. Generator Power
3. UPS Power
4. Branch Circuit Power
5. Branch Circuit Energy
6. Power Losses
7. PUE

Check the "Help -> About" section in Management Console to determine what modules are licensed on the machine.


Resolution:
Please contact your local distributor to purchase additional modules. 

The following part numbers are only compatable with PME 7.2.x Data Center Edition
 
Part Number Report Description
IE7MGNCZZSPEZZ Generator Power Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MPNCZZSPEZZ Power Losses Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MRNCZZSPEZZ Branch Circuit Power Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MSNCZZSPEZZ Branch Circuit Energy Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MTNCZZSPEZZ Generator Test Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MUNCZZSPEZZ UPS Power Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
IE7MWNCZZSPEZZ PUE Add-on Module for StruxureWare Power Monitoring Expert DataCenter Edition
Was this helpful?
What can we do to improve the information ?