Technical FAQs

Ask a Question

What is the luminance or brightness of the HMIGTU targets?

Issue:
What is the luminance or brightness of the HMIGTU targets?
 
Product Line:
Magelis HMIGTU
 
Environment:
 
 
Cause:
 
 
Resolution:
Below are the HMIGTUs brightness rating in candela per squared meter (cd/m2):
HMIDT732 = 326 cd/m2
HMIDT643 = 266 cd/m2
HMIDT642 = 266 cd/m2
HMIDT542 = 264 cd/m2
HMIDT651 = 226 cd/m2
HMIDT551 = 360 cd/m2
HMIDT351 = 266 cd/m2
Was this helpful?
What can we do to improve the information ?