Technical FAQs

Ask a Question

What is the replacement CT"s part number on a ATS48C66Y soft start?

Issue:
What is the replacement CT"s part number on a ATS48C66Y soft start?
Product Line:
Altistart ATS48
Environment:
All
Cause:
Replacement parts needed.
Resolution:
CT's are part of the bus bar assembly VZ3N005S48 however this part is not available to purchase. One option is to return the Soft Start for repair.
Was this helpful?
What can we do to improve the information ?