Technical FAQs

Ask a Question

Are Micom relays RoHS compliant?

Title
Are Micom relays RoHS compliant?

Issue
Unable to find out if Micom relays RoHS Compliant

RoHS Compliance Definition
The definition and aim of the RoHS directive is quite simple. The RoHS directive aims to restrict certain dangerous substances commonly used in electronic and electronic equipment. Any RoHS compliant component is tested for the presence of Lead (Pb), Cadmium (Cd), Mercury (Hg), Hexavalent chromium (Hex-Cr), Polybrominated biphenyls (PBB), and Polybrominated diphenyl ethers (PBDE). For Cadmium and Hexavalent chromium, there must be less than 0.01% of the substance by weight at raw homogeneous materials level. For Lead, PBB, and PBDE, there must be no more than 0.1% of the material, when calculated by weight at raw homogeneous materials. Any RoHS compliant component must have 100 ppm or less of mercury and the mercury must not have been intentionally added to the component. In the EU, some military and medical equipment are exempt from RoHS compliance.

Product Line

Micom relays, Energy products

Environment
Energy products

Cause
Unable to find out if Micom relays or any other products are RoHS Compliant

Resolution
Below is the  link (on SE Web site) where you can enter all product name, and you have all info on ROHS for all devices:
http://www2.schneider-electric.com/sites/corporate/en/products-services/green-premium/check-a-product.page


 
Was this helpful?
What can we do to improve the information ?