Technical FAQs

Ask a Question

Does the embedded Ethernet port on the M340 processors (BMXP342020 or BMXP342030) support the ODVA Ethernet/IP protocol ?

No. The embedded Ethernet port on the M340 processors (BMXP342020 or BMXP342030) only supports the ModbusTCP protocol.
Was this helpful?
What can we do to improve the information ?