Technical FAQs

Ask a Question

What is the pin out of the programming cable to connect to a Twin Line drive/controller from a PC?

Title:  What is the pin out of the programming cable to connect to a Twin Line drive/controller from a PC?


Issue:  There is a need to connect to the Twin Line drive / controller to configure, change parameters or for troubleshooting purposes.


Product Line:  Twin Line Drive / Twin Line Controller


Environment:  None


Cause: The programming cable bearing part number TLACDPBGxxx is obsolete and no longer available.


Resolution:

The programming cable to connect to the Twin Line drive / controller is a standard RS232 cable. It can be either procured from external sources (or) a cable may be made using the pin out details provided below.

 

Was this helpful?
What can we do to improve the information ?