Technical FAQs

Ask a Question

How can I correct Proworx error "Error Opening Database MCUserTCop.mdb Repair: "MDIForm1.frm method=iEHTimer_Timer err=440 automation error"?

This error is caused when the user does not have full access rights to the PLC.
In addition, the user can right click on the Proworx icon and 'run as administrator' if running Windows 7.
Was this helpful?
What can we do to improve the information ?