Technical FAQs

Ask a Question

How many IO Scanner connections are supported by the M580 BMENOC03x1 Ethernet modules?

The M580 Ethernet modules BMENOC0301 and the BMENOC0311 each support a maximum I/O scanner configuration of 128 devices or connections (Shared by EtherNet/IP and Modbus TCP).
Was this helpful?
What can we do to improve the information ?