Technical FAQs

Ask a Question

Does the Magelis Panel PC, HMIPPH7D0701, has an option for RS485?

Issue:
Does the Magelis Panel PC, HMIPPH7D0701, has an option for RS485?
 
Product Line:
Magelis Panel PC, HMIPPH7D0701
 
Environment:
 
 
Cause:
 
 
Resolution:
 The 15-inch Panel PC part number HMIPPH7D0701 does not have an RS485 card option.  Our recommendation would be to go with the BOX PC as that range has a RS-485 option module.  Or the 12-inch Panel PC targets which also has a RS-485 option module. 
Was this helpful?
What can we do to improve the information ?